User Interface
User interface function allows you to customize the appearance of the display and displayed parameters.
You can choose:
-
Temperature units
-
Language and PIN code
-
Theme and screensaver
-
Brightness level
-
Type and brightness of the screensaver
You can set the time for the screen to turn off when idle (Turn off screen after parameter). If you set the value to "0 s", you can turn the screen on and off through a 1-bit object.
If you do not want the screen to be just dark when off, enable the screen saver function.
The screensaver interface displays an electronic clock, images, or custom text with a maximum of 18 English or 6 Chinese characters. If there are cedillas or other special characters in the description that consist of more than one-byte character, the maximum number of characters depends on the number of cedillas or special characters.
You can also set the back light percentage and the delay time for activating the screen saver.