MTN6215-0410S_SW_EN_EU_2024_06_05

Fan

In the Fan tab, you can set values for the fan speed. You can check the Automatic operation function however, you can still control the fan speed manually on the screen.


You can choose from 2 formats for 1byte object:

  • Number between 0 and 255

  • Percentage value 0 – 100 %

There are values set as default in the ETS. You can use them or change them later as needed.

The value you set as the output value for each speed is shown on the display via Fan speed, status object.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?