MTN6215-0410S_SW_EN_EU_2024_06_05

Internal Temperature

The internal temperature is displayed based on the value from the internal temperature sensor. There is no special internal temperature group object for the Air quality display.

Function 1

Type of air quality display

Int. temperature

Text for unit

°C

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?