Group Objects
The blinds are moved via the Up/Down, moving object.
The blinds are stopped and adjusted via the Stop/Slat, adj. object.
The status indication is controlled via Slat position, status and Blind position, status object.
The Blind position and Slat position object send the value to the bus when you drag the bar on the screen to set the position level.
|
No. |
Name |
Object function |
Length |
Behavior |
Data Type |
|---|---|---|---|---|---|
|
244 |
Screen 1 Function 1 |
Up/Down |
1 bit |
Sends |
1.008 up/down |
|
245 |
Screen 1 Function 1 |
Stop/Slat adj. |
1 bit |
Sends |
1.007 step |
|
246 |
Screen 1 Function 1 |
Blind position |
1 byte |
Sends |
5.001 percentage (0..100%) |
|
247 |
Screen 1 Function 1 |
Slat position |
1 byte |
Sends |
5.001 percentage (0..100%) |
|
249 |
Screen 1 Function 1 |
Blind position, status |
1 byte |
Sends, Receives, Updates |
5.001 percentage (0..100%) |
|
250 |
Screen 1 Function 1 |
Slat position, status |
1 byte |
Sends, Receives, Updates |
5.001 percentage (0..100%) |