Setting Rules for the PI Control
Large system increases (e.g., high heating output, steep characteristic curves for valves) are controlled with large proportional ranges.
Slow heating systems (e.g., underfloor heating) are controlled with high-level reset times.
Adjustment via control parameter
If no satisfactory control result is achieved by selecting an appropriate heating or cooling system, you can improve the adaptation via control parameters.
|
Low proportional range |
Large overshoot for setpoint changes (also continuous oscillation under certain circumstances), rapid adjustment to the setpoint. |
|
Large proportional range |
No (or little) overshooting, but slow adjustment. |
|
No reset time |
Rapid correction of control deviations (ambient conditions), risk of continuous oscillation. |
|
Long reset time |
Slow correction of control deviations. |
The framework conditions for setting the cycle time
-
For small values, the switching frequency and the bus load are increased.
-
For large values, temperature fluctuations are created in the room.
-
Short cycle time for rapid heating systems (e.g., electric heating).
-
Long cycle time for slow heating systems (e.g., underfloor warm water heating).
Examples
Warm water radiator heating with motorized valve drives
|
Properties |
Parameter |
Settings |
|---|---|---|
|
Heating only |
Controller type |
Heating |
|
Control value output |
Continuous PI control |
|
|
Adjusting the controller to the heating system |
Hot-water heating (5 K / 150 minutes) |
|
|
Send control value on change by |
4 % |
|
|
Cyclically send control value |
10 minutes |
Cooling ceiling with motorized valve drives
|
Properties |
Parameter |
Settings |
|---|---|---|
|
Cooling only |
Controller type |
Cooling |
|
Control value output |
Continuous PI control; |
|
|
Adjusting the controller to the cooling system |
Adjustment via control parameter |
|
|
Cooling proportional range |
Approx. 30 °C(depending on the application) |
|
|
Reset time for cooling |
Approx. 240 min. (depending on the application) |
|
|
Send control value on change by |
4 % |
|
|
Cyclically send control value |
10 minutes |
Switching electric radiator heating
|
Properties |
Parameter |
Settings |
|---|---|---|
|
Heating only |
Controller type |
Heating |
|
Control value output |
Switching PI control |
|
|
Adjusting the controller to the heating system |
Electric heating (4 K / 100 min.) |
|
|
Send control value on change by |
4 % |
|
|
Cyclically send control value |
10 min. |
Air conditioning with 4-duct (2-circuit) air convector system (e.g., switching valve drives)
|
Properties |
Parameter |
Settings |
|---|---|---|
|
Heating or cooling as required, with automatic switching |
Controller type |
Heating and cooling |
|
Control value output – heating |
E.g. switching PI control |
|
|
Adjusting the controller to the heating system |
Split unit (4 K / 90 min.) |
|
|
Control value output – cooling |
E.g. switching PI control |
|
|
Adjusting the controller to the cooling system |
Electric heating (4 K / 100 min.) |
|
|
E.g., automatically switch between heating and cooling |
Switch between heating and cooling |
Automatically via the controller |
Temperature limitation using shading facility
|
Properties |
Parameter |
Settings |
|---|---|---|
|
Cooling only |
Controller type |
Cooling |
|
Control value output – heating |
Switching 2-step control |
|
|
Hysteresis |
Large (e.g. 10 °C) |