MTN6215-0410S_SW_EN_EU_2024_06_05

Heating and Cooling

You can set how the change between heating and cooling takes place using the Heating/Cooling switchover parameter.

  • Automatically by the controller

  • Set externally via the Heating/cooling mode object

  • Via button

  • Via both button and object

Automatic Changeover

If you select the Automatic changeover between Heating and Cooling, the controller decides which mode is suitable based on the parametrized setpoints, the insensitive zone and the current actual temperature.

If you select the external switchover using Heating/cooling mode object, the controller can only be forced into heating or cooling mode by the object value.

NOTE: The status of an external device for changing over between heating and cooling can be interrogated.
To do this, set the Read on init flag on the Heating/cooling value object.
The external unit is operational after a reset and supports the read request. Also set cyclical sending on the external device.

Dead Zone

The insensitive zone prevents the controller from switching frequently between heating and cooling. For example, if a heater is used for heating, it has sufficient thermal energy after the valve has been closed to continue to heat the room above the setpoint temperature.

Example:

If you have project the same value for the heating and cooling setpoints, the insensitive zone is set to "0 K". After a delay time that can be set has elapsed, the air conditioning system cools because the setpoint for cooling has been exceeded. If there is a short delay time, the controller switches the controller mode particularly frequently.

Make sure that the heating setpoint is always less than the cooling setpoint.

Status after Power on/Download

You define the mode to which the controller changes after download (Heating or Cooling) or reset (Heating/Cooling/As before voltage failure).

2-Pipe/4-Pipe HC System

Finally, you choose between a 2-pipe and a 4-pipe system.

In the 2-pipe system, heating and cooling mediums (depending on the season) are lead through the same lines and controlled via the same valve.

2-pipe HC system

A Cooling supply

B Heating supply

C Cooling return

D Heating return


4-pipe HC system

A Cooling supply

B Heating supply

C Cooling return

D Heating return


The changeover between heating and cooling medium is performed by the system, and must therefore be passed on to the controller.

The Heating/cooling mode object sends “0” for heating mode and a 1 for cooling mode to the actuator.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?