MTN6215-0410S_SW_EN_EU_2024_06_05

Move the Blinds

Drag the bar on the screen to move the blind either up or down and adjust the slats. When you release the bar, the moving process stops (via Stop/slat adj. object).

The blind is moved up or down via the 1-bit Up/Down object. If the Up/Down object has the value of “1” (down), the value after the next long press is “0” (up) and vice versa.

With Blind position function, in addition to opening and closing, you can adjust the position of the curtains/blinds to the certain value (0 to 100 %).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?