MTN6215-0410S_SW_EN_EU_2024_06_05

Automatic Operation

If you enable Automatic operation function, the fan coil actuator takes over control of the fan steps. You can still control the fan speed manually on the screen.

Function 1

Automatic operation function

Enable

Automatic operation is controlled by Fan automatic operation object and displayed via Fan automatic operation, status group object.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?