Shift without Step Value
If you choose the option Shift without step value, you can set up to 10 different values for each shift (Shift value). You send a value with each button action (short press). If, for example, you want to send 5 values with the button, press the button 5 times.
|
Function x |
Shift type |
Shift without step value |
|
|
Shift number |
1 – 10 |
||
|
Value 1 |
0 – 255 |
||
|
..Value 10 |
0 - 240 |
Shift direction: The values are sent one after the other in the order you choose (increase or decrease).