MTN6215-0410S_SW_EN_EU_2024_06_05

Continuous PI Control

For the continuous PI control, the corresponding 1-byte control value is transmitted 0 – 100 % directly via the bus to the heating actuator or a valve drive, which convert the control value directly to a degree of opening. However, this is only transmitted when the newly calculated control value has changed by a specified percentage.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?