MTN6215-0410S_SW_EN_EU_2024_06_05

FCU Controller

In the FCU controller sub-menu you can set the parameters for measuring and evaluating the temperature, select the function mode (heating/cooling) and you can even link the FCU module with a bus presence detector or sensors in the windows.

The actual temperature can be registered using various temperature sensors:

  • Internal sensor of the controller

  • External sensor, the values of which are received by the External temperature sensor object

  • Internal sensor combined with external

The controller can evaluate 2 temperatures proportionately from 0‑100 %.

You can also set the control mode and interval for sending the measured values and the control value in case of a measurement error.

Power on/off status: With this setting, you can choose how the FCU controls the status after the download is complete and the device is powered on (again).

Function configuration

FCU controller

Power on/off after download

Off/On

Power on/off status after voltage recovery

Off/On/Before voltage failure

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?