MTN6215-0410S_SW_EN_EU_2024_06_05

Scene

It is possible for a device to act as a scene controller. It sends a value to each channel that needs to be controlled and it can receive a scene command from another device or Scene group module (see Scene Group).

Assign a number (1 to 64) to the scene, name it and select an icon.

Express settings

Function

Scene

Screen 1

Function name

1 – 8 characters (≤20 English or 6 Chinese characters)

Function 1

Icon preview

 
   

Function icon

 
   

Colour of function icon indication when status ON

Green/White

   

Colour of function icon indication when status OFF

Green/White

   

Scene number

1 – 64

   

Storage scene via long operation

Enable/Disable

   

Object with status feedback

Enable/Disable

You can configure a long press of the button (≥ 2 s) to initiate a save scene command. This stores the current setting into the scene.

There are two ways how to set up the status feedback:

  1. Simple feedback: User gets feedback about the scene when they push the button. The actuator stays out of this.

  2. Status of the actuator is linked with icon status feedback: Icon status and status of the actuator are synchronized.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?