Temperature Setting
You can set temperature limits and the step value for temperature adjustment. Tapping on a button increases or decreases the setpoint in increments of 0.5 °C or 1 °C.
To be able to increase and decrease the temperature in this way, you must link the following objects to the appropriate group address:
-
146 FCU – Current setpoint adjustment
-
164 FCU – Current temperature setpoint
The setpoint can only be changed up to the limits that apply to the room temperature control unit in question.
|
FCU controller |
Setpoint temperature adjustment step |
0,5 / 1 °C |
|
|
Min. set temperature |
5 – 37 °C |
||
|
Max. set temperature |
5 – 37° C |
The minimum temperature has to be set lower than the maximum.
If the user sets a temperature that exceeds the original minimum/maximum, this temperature is considered the new minimum/maximum.