MTN6215-0410S_SW_EN_EU_2024_06_05

PM10

To display the concentration of the particulate matter, you can select either the value in μg/m3 or the concentration expressed as a floating value.

You can name your unit and set the requesting time interval.

Function 1

Type of air quality display

PM10

Object datatype

Value in μg/m3 (DPT 7.001)

Float value in μg/m3 (DPT 9.030)

   

Text for unit

"5 bytes allowed"

   

Time period for request external sensor

0 – 255 min

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?