Internal and External Temperature Sensor
The device has a built-in internal temperature sensor. However, you can also select an external sensor that sends values to the controller via the bus. The bus then evaluates the current temperature.
|
Function 1 |
Interface display temperature |
Setpoint temperature |
||
|
Actual temperature |
||||
|
Room temperature reference from |
Internal/Internal sensor |
|||
|
Time period for request external sensor |
0 – 255 min |
You can set the time interval for the device to send a temperature read request to an external temperature sensor (after the bus is reset or programmed).
All the past temperature data get erased.
The device works with new data received from the bus during the time interval.