MTN6215-0410S_SW_EN_EU_2024_06_05

Air Conditioner Control Panel

With Air conditioner function you can regulate the air temperature (heating/cooling, fan speed) and humidity.

Express settings

Function

Air conditioner

Screen 1

Function name

1 – 8 characters (≤20 English or 6 Chinese characters)

Function 1

Icon preview

 
   

Function icon

 
   

Colour of function icon indication when status ON

Green/White

   

Colour of function icon indication when status OFF

Green/White

The Interface display temperature function shows setpoint or actual temperature values on one screen.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.