MTN6215-0410S_SW_EN_EU_2024_06_05

Logic Function

In complex KNX installations, the logic function serves to establish special logic operations between sensors and actuators. There is a wide range of possible settings for executing numerous logic functions for controlled KNX devices (e.g. dimming or switch actuators, various sensors etc).

The logic function is particularly suitable for summarizing messages (e.g. the lighting status in rooms), linking conditions (e.g. rain or wind sensor activates a safety function) or programming an additional toggle between manual and automatic (e.g. disabling brightness-dependent lighting control for a video presentation).

Due to the large number of possible settings, the logic module is particularly well suited to the areas of security, comfort or energy saving.

The outputs can also be shown on the visualization device.

By default, all 8 possible logic functions/blocks are deactivated. You have to enable the required amount of the functions.

Logic functions

1st Logic function

Enable

1st Logic

   

You can choose from one of the following logic operations for each logic block.

1st Logic

Function of channel

AND

OR

XOR

Threshold comparator

Format convert

NOTE: Always set all parameters on the first block before parameterizing the next block.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?