MTN6215-0410S_SW_EN_EU_2024_06_05

Heating and Cooling Control

The room temperature control unit transmits values to the bus via various group objects, which you can use to control different controller types with switching commands or by specifying percentage values:

  • Switching on/off (use 2-point control)

  • Switching PWM (use PI control)

  • Continuous control (use PI control)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?