MTN6215-0410S_SW_EN_EU_2024_06_05

RGB/W Dimming

The RGB/W dimming function is an extended dimming function for KNX devices that supports color control.

The user calls up the set lighting color by pressing the button (for example via an RGB/W KNX actuator or a KNX DALI-Gateway).

In ETS, you set the RGB/W value, download the setting to the device and connect it to a specific button.

Express settings

Function

RGB dimming

RGBW dimming

Screen 1

Function name

1 – 8 characters (≤20 English or 6 Chinese characters)

Function 1

Object datatype

1 x 3 byte / 3 x 1 byte

1 x 6 byte / 4 x 1 byte

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?