MTN6215-0410S_SW_EN_EU_2024_06_05

Scenes

You have the option of linking the ventilation with up to five scenes, for which you can set the parameters independently. To do this, use the 1-byte Scene object.

If you enable the Heat recovery function in Function menu, you can adjust the Heat recovery parameters in the Scene sub-menu.

Function 1

1 – 5 → Assign scene NO.

1– 64, 0 = inactive

Scene

Fan

Unchange

OFF

Low

Medium

High

Heat recovery

Unchange

OFF

ON

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?