MTN6215-0410S_SW_EN_EU_2024_06_05

Play Mode

For each play mode, you can specify the output and status values (range 0 – 255). The output value is the one you send to the actuator and the status value is the one visible on the screen (via Play mode, status group object).

Function 1

Play mode

Enable

Play in single cycle mode

Output value for play in single cycle mode (0 – 255)

Status value for play in single cycle mode (0 – 255)

 

Play in order mode

Output value for play in order mode (0 – 255)

Status value for play in order mode (0 – 255)

   

Play in random mode

Output value for play in random mode (0 – 255)

Status value for play in random mode (0 – 255)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?