MTN6215-0410S_SW_EN_EU_2024_06_05

Internal and External Temperature Sensor

The device has a built-in internal temperature sensor. However, you can also select an external sensor that sends values to the controller via the bus. The bus then evaluates the current temperature.

Function 1

Controller from

External

 

Interface display temperature

Setpoint temperature

 

Actual temperature

 
   

Room temperature reference from

Internal/Internal sensor

     

Time period for request external sensor

0 – 255 min

You can set the time interval for the device to send a temperature read request to an external temperature sensor (after the bus is reset or programmed).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?