MTN6215-0410S_SW_EN_EU_2024_06_05

Heat Recovery

With active monitored ventilation, a ventilation blows fresh air into the building and extracts the consumed air. The goal of the heat recovery process is to extract thermal energy of the discharged air (e.g. via a cross-flow heat exchanger) in order to warm up the “fresh” air with it.

Heat sources inside a building (e.g. lighting, computers) can also help with heating which contributes to an increase in energy savings.

Function 1

Heat recovery function

Enable

Heat recovery function is controlled by KNX fan coil actuator/controller via 1-bit Heat recovery object. The screen displays the status of heat recovery process via 1-bit Heat recovery, status object (on/off).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?