MTN6215-0410S_SW_EN_EU_2024_06_05

Advanced Functions

In the Advanced functions tab, you can extend the device functionality with HVAC, Logic, and Scene group controllers. You check the appropriate box and then set the required parameters in the main menu. See more in HVAC Controller.

Advanced function

HVAC controller

Enable/Disable
 

Logic function

 

Scene group function

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?