MTN6215-0410S_SW_EN_EU_2024_06_05

External Temperature

External temperature is displayed based on values from the external temperature sensor. You can set the interval for requesting values via the bus.

Function 1

Type of air quality display

Ext. temperature

Text for unit

°C

   

Time period for request external sensor

0 – 255 min

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?