MTN6215-0410S_SW_EN_EU_2024_06_05

Group Objects

Energy data is received from the bus and displayed on the screen, 4 bytes, kWh (DPT 13.013).

No.

Name

Object function

Length

Behavior

Data Type

244

Screen 1 Function 1

Active energy value

4 byte

Sends, Receives, Updates

13.013 active energy (kWh)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?