HVAC Controller
The device integrates the Heating, Ventilation and Air-Conditioning to a coherent and efficient climate control. Measured temperature values in the rooms are recorded and supplied to the heating/cooling and ventilation control to generate the optimum temperature and air quality, using fresh air from outdoors.
The HVAC module supports room temperature and ventilation control.
|
HVAC controller Controller settings |
FCU controller |
Enable |
|
|
Floor heating controller |
|||
|
Ventilation controller |
Turn off the thermostat before ETS download, reset, or micro-USB update. This is to prevent the HVAC system from being driven by a not stabilized built-in temperature sensor.
You can deactivate the thermostat by the ON/OFF icon on the respective screen. It is also recommended to set Power on/off after download to OFF in FCU and Floor Heating controller in ETS before download.
-
HVAC controller > FCU controller > Power on/off after download > OFF
-
HVAC controller > Floor heating controller > Power on/off after download > OFF