MTN6215-0410S_SW_EN_EU_2024_06_05

CO2

The carbon dioxide content values in the air come from the external sensor. You can select from two types of units to display on the screen: Either a value in ppm or a floating value in ppm.

You can name your unit and set the requesting time interval.

Function 1

Type of air quality display

CO2

Object datatype

Value in ppm (DPT 7.001)

Float value in ppm (DPT 9.008)

   

Text for unit

"5 bytes allowed"

   

Time period for request external sensor

0 – 255 min

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?