Group Objects
Switching is carried out via the Switch object or the Brightness dimming object.
Dimming is carried out via the Brightness dimming object.
A dimming function requires minimal 2 group addresses. The first group address links the switching objects of the device with the switching objects of the dimmer channel. The second group address links the dimming objects of the device with the dimming objects of the dimmer.
The status indication is controlled via the Switch, status and Brightness, status objects.
|
No. |
Name |
Object function |
Length |
Behavior |
Data Type |
|---|---|---|---|---|---|
|
244 |
Screen 1 Function 1 |
Switch |
1 bit |
Sends |
1.001 switch |
|
246 |
Screen 1 Function 1 |
Brightness dimming |
1 byte |
Sends |
5.001 percentage (0..100%) |
|
249 |
Screen 1 Function 1 |
Switch, status |
1 bit |
Sends, Receives, Updates |
1.001 switch |
|
251 |
Screen 1 Function 1 |
Brightness, status |
1 byte |
Sends, Receives, Updates |
5.001 percentage (0..100%) |