Shift by Step Value
You can set the start/end value of the shift and the size of the step. Short button press then triggers the whole cycle of steps.
|
Function x |
Shift type |
Shift by step value |
|
|
Lowest value with |
0 – 240 |
||
|
Highest value with (must be larger than lowest value with) |
1 – 250 |
||
|
Step size |
0 - 240 |
The shift direction can be set from highest to lowest (decreases) or from lowest to highest (increases). It changes by the size of the step you choose.
In the default setting, the object value is raised by the value "2" if you release the button before the long operation time elapses.