Volume
You can select either a 1-bit or a 1-byte object datatype to control the volume.
|
Function 1 |
Control mode of volume adjustment |
1 bit (relative control) 1 byte (absolute control) |
|
|
Object datatype |
Percentage (DPT 5.001) Percentage (DPT 5.004) |
||
|
Max. volume value |
10 – 100 % |
With a 1-bit object (Volume + = 1/Volume – = 0), you can change the volume one step up or down (relative control):
-
1 = one step up
-
0 = one step down
Absolute control means that you adjust the volume level on a scale by dragging the bar on the screen. You can choose whether the volume is transmitted as a percentage (DPT 5.001) or as a percentage (DPT 5.004) from 0 – 100 %.