MTN6215-0410S_SW_EN_EU_2024_06_05

Appropriate ETS Version

The application is suitable for the ETS5. You cannot use earlier versions, e.g., the ETS3, ETS4.

Application files (knxproj) are optimised for the relevant ETS version. If you load an ETS4 application to ETS5, time will be wasted on conversion.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?