MTN6215-0410S_SW_EN_EU_2024_06_05

Power On/Off after Download/Voltage Recovery

If the bus voltage fails but the power supply is running, the device continues to operate normally and saves the internal values.

If the power failure exceeds the backup time, the device shuts down safely.

When power has been restored, the device restarts.

You can define the status of the Room temperature control function on voltage recovery and after download.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?