MTN6215-0410S_SW_EN_EU_2024_06_05

Input/Output Behavior

The first block of functions is described together, because all three operations have the same parameters and values.

Input behavior

You can use up to 8 inputs (a – h). By default, all the inputs are disconnected.

The input telegrams can be inverted for each input. In addition, a fixed value (0 or 1) can be assigned.

1st Logic

Function of channel

AND

Input a-h

Disconnected

Normal

Inverted

   

Default value

0

1

Output behavior

Criteria for the sending behavior at the output can be defined.

1st Logic

Result is inverted

No/Yes

Read input object value after bus voltage recovery

No/Yes

   

Output send when

Receiving a new telegram (on the input)

Every change of output object

   

Send delay time: Base

None - 25 s

   

Factor: 1..255

1 -255

If you click Yes for Read input object value after bus voltage recovery, the logic module sends a read telegram to all inputs asking about their values.

If one or more inputs do not respond, the bus keeps on trying to collect missing responses. Output send when option allows you to set whether the output should be sent after receiving a new telegram at the input or at every change of the output object.

This setting is wise if a rapid response is expected (e.g. weather alarm at the blind actuator). This function also helps to prevent bus overload.

Example:

  • A light-sensitive switch switches the lighting on automatically.

  • The light is switched off between 23:00 and 06:00.

  • In the morning, the light switches on from 06:00 when it is dark.

  • In addition, the light can be switched on for 5 minutes at any time via a push-button.

  • A continuous light function is possible for maintenance purposes.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?