MTN6215-0410S_SW_EN_EU_2024_06_05

PIN Code

If you activate the screen access function, you can set a four-digit security password and select the output object value sent to the bus after entering the password. You can set up sending with a delay. Once you input the correct password, the device exits from the screen saver to normal mode.

The preset PIN code combination is 1234. Screen access becomes disabled if you set an invalid PIN code (for example, 1234, 1111, or 2222).

User interface

Use screen access pin code

Check (Yes)

Password setting

4 digits: 0 – 9

 

Output object type when input pin code

No reaction

1 bit (On/Off)

1 byte (scene control): 1 – 64

1 byte: 0 – 255

1 byte: 0 – 100 %

   

Delay time for sending

0 – 255 s

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.