MTN6215-0410S_SW_EN_EU_2024_06_05

Scene Group

The scene module allows you to set a wide number of combinations to control large units (e. g., switch off all lamps in huge public areas, move up all the blinds in office buildings).

If you enable the Scene group function, you can set up to 8 scene groups, each of which you can independently assign different values and set specific parameters.

Scene group

Scene group settings

Scene group function

Enable

 

Scene group 1 function

Disable/Enable

Each scene group has 8 outputs. For each of them, you can define 6 scene numbers. Within each Scene group, you can define 48 scenes. You can assign a scene number 384 times in total.

Scene group settings

Scene group 1

G1: Output 1 – 8 function

 

Enable

Object type of output

1 bit / 1 byte / 2 byte

 

1 – 6 output 1 trigger scene NO. is

1 – 64 (0 = inactive)

   

Object value of output 1

1 / 0

   

Delay time for sending

0 – 63 * 0,1 s

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?