MTN6215-0410S_SW_EN_EU_2024_06_05

Color Temperature Dimming

The Color temperature dimming function transmits values for setting the color temperature in Kelvin via the external device.

Pressing the button transmits 2 bytes of absolute color temperature values.

You can set the minimum and maximum values and the step width by which you increase or decrease temperature.

Express settings

Function

Colour temperature dimming

Screen 1

Function name

1 – 8 characters (≤20 English or 6 Chinese characters)

Function 1

Increase/Decrease step width

100, 200, 500, 1000 K

   

Min. color temperature

1000 – 10000 K

   

Max. color temperature

1000 – 10000 K

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?