Group Objects
The Main scene trigger object receives the scene number (1 – 64) from one of the buttons or another sensor. Then all outputs with that specific scene number send out the object (1 bit, 1 byte, 2 bytes).
|
No. |
Name |
Object function |
Length |
Behavior |
Data Type |
|---|---|---|---|---|---|
|
6 |
Scene Group |
Main scene trigger |
1byte |
Sends, Receives |
17.001 scene number |
|
7 |
1st Scene Group |
Sub scene output 1 |
1bit 1byte 2byte |
Sends |
1.001 switch 5.010 counter pulses 7.001 pulses |
|
8 |
Sub scene output 2 |
||||
|
9 |
Sub scene output 3 |
||||
|
10 |
Sub scene output 4 |
||||
|
11 |
Sub scene output 5 |
||||
|
12 |
Sub scene output 6 |
||||
|
13 |
Sub scene output 7 |
||||
|
14 |
Sub scene output 8 |