MTN6215-0410S_SW_EN_EU_2024_06_05

Positions of Slats

You can adjust blind to various opening angles. However, the symbol for the slat position does not reflect the actual opening angle.

The slat position reached with a position value depends on the particular blind.

There are blinds with an opening angle of 180° which move up and down when the slats are positioned vertically. When the position value is 50%, the slats are horizontal.

Other blinds have an opening angle of 90° and move up when the slats are positioned horizontally, and down when the slats are positioned vertically.

These blinds turn to the horizontal position with the value 0% and to the half-opened position with the value 50%.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?