MTN6215-0410S_SW_EN_EU_2024_06_05

Brightness

To display the brightness level, you can select either the value in lux or as a floating value in lux.

You can name your unit and set the requesting time interval.

Function 1

Type of air quality display

Brightness (lux)

Object datatype

Value in lux (DPT 7.013)

Float value in lux (DPT 9.004)

   

Text for unit

"5 bytes allowed"

   

Time period for request external sensor

0 – 255 min

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?