MTN6215-0410S_SW_EN_EU_2024_06_05

Move Curtain/Roller

Drag the bar on the screen to move the curtain or roller up or down to a certain level and the slat angle.

For complete closing/moving down, the Open/Close or Up/Down object sends the value “1”, and it sends the value “0” for opening/moving up.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?