MTN6215-0410S_SW_EN_EU_2024_06_05

Control Mode

You can choose from four control modes.

Function 1

Control mode

Heating

Cooling

Heating and Cooling

Heating and Cooling (with auto mode)

The device provides the setpoint and current room temperature to the heating/cooling unit.

Modes:

If you choose the Heating/Cooling option, you can manually switch between heating and cooling via Heating/Cooling mode group object and see the status on the screen (via Heating/Cooling mode, status group object).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?