Room Temperature Control Panel
Room temperature control panel function offers the possibility of regulating the room temperature of a single room regardless of the temperature in other rooms.
The setting is very similar to the Air conditioner setting.
See also Air Conditioner Control Panel.
|
Express settings |
Function |
Room temperature unit |
|
|
Screen 1 |
Function name |
1 – 8 characters |
|
|
Function 1 |
Controller from |
Local (FCU controller) Local (Floor heating controller) External |
If you select Local controller (FCU or Floor heating), a warning appears to activate the corresponding function in the HVAC controller menu.
If you select an external controller, you can set the required parameters directly in the Room temperature control panel menu.