MTN6215-0410S_SW_EN_EU_2024_06_05

Audio Control

Audio control function allows you to control music playback. You connect device group objects to a KNX music server and set the function parameters in ETS.

Express settings

Function

Audio control

Screen 1

Function name

1 – 8 characters (≤20 English or 6 Chinese characters)

Function 1

Icon preview

 
   

Function icon

 
   

Colour of function icon indication when status ON

Green/White

   

Colour of function icon indication when status OFF

Green/White

You can set the volume control method and play mode, enable the Mute and Track name function.

Function 1

Control mode of volume adjustment

1 bit (relative control)

1 byte (absolute control)

 

Mute

 
 

Track name

 
   

Play mode

 

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?