MTN6215-0410S_SW_EN_EU_2024_06_05

Ventilation System

A ventilation system adjusts ventilation rates in time or by location in a building to be responsive to selected parameters.

In addition to the baseline values, the values for the room temperature, air humidity, and CO2 and PM2,5 content can be transferred via the KNX interfaces to the ventilation system and taken into account during the control.

Ventilation systems can also have sensors to detect airflow, system pressure, or fan energy use in such a way that systems failures can be detected and repaired, as well as when system components need maintenance, such as filter replacement.

Express settings

Function

Ventilation system

Screen 1

Function name

1 – 8 characters (≤20 English or 6 Chinese characters)

Function 1

Icon preview

 
   

Function icon

 
   

Colour of function icon indication when status ON

Green/White

   

Colour of function icon indication when status OFF

Green/White

You can define the status of the ventilation system on bus voltage recovery and after download and choose the default fan speed after the ventilation is back on.

Function 1

Power on/off after download

OFF/OF

 

Power on/off after voltage recovery

OFF

ON

Before voltage failure

 

Default fan speed after ventilation on

Low

Medium

High

Last status

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?