Process Framework Caching and the Transition Node Action Handler

By default, the Process Framework architecture caches the states of nodes that it has accessed. This is done to improve performance for the desktop Process Framework applications (e.g., Session Manager, Workflow Manager). However, this behavior may cause an undesirable effect within Geodatabase Manager.

For example, suppose a version related to a session node is processed by Geodatabase Manager, but is found to have conflicts and subsequently transitioned to a state called 'In Conflict.' On another computer, a user opens the In Conflict session, resolves any conflicts, and then resubmits the session to be posted, which includes transitioning the session from the 'In Conflict' state to a 'Pending Post' state. Depending on various circumstances, the Process Framework application instance that Geodatabase Manager uses to access session nodes may still consider that session to be in the 'In Conflict' state, because the transition was not performed within its context. This may result in some configured Process Framework tasks or action handlers to not process the version or node appropriately.

The ArcFM Solution provides a means to disable the Process Framework caching behavior using a registry key on the computer that hosts the Geodatabase Manager service. This key notifies the Process Framework to not cache node states. On a 32-bit system, install this registry key using the Disable_CSCache.reg file that is installed along with Geodatabase Manager in the following directory: \Program Files\Miner and Miner\ArcFM Solution\bin\. On 64-bit systems, you need to edit the registry subkey in this .reg file. With Disable_CSCache.reg open in a text editor like Notepad, edit the subkey [HKEY_LOCAL_MACHINE\SOFTWARE\Miner and Miner\Process Framework\Caching] to read [HKEY_LOCAL_MACHINE\SOFTWARE\Wow6432Node\Miner and Miner\Process Framework\Caching] instead. Save the file and double-click to create the registry key.

IMPORTANT: Schneider Electric recommends that you disable the Process Framework caching behavior on any machine used to host a Geodatabase Manager service.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.