Open Redline Design

Opens a design for redline (graphic) editing in ArcFM Viewer for ArcGIS Engine.

Enabled

  • A design node must be selected.

  • MMWorkflowManager must be the current extension.

  • The design may not have a state of Verified.

  • Workflow Manager must be open from ArcFM Viewer for ArcGIS Engine and visible.

Execute

  1. Gets the design.

  2. Creates a Mobile packet if one does not already exist for the design.

  3. Determines whether the design should be opened as View Only.

  4. Loads the design's stored display (if it exists).

  5. Loads the design's Mobile packet.

  6. Activates the mobile graphics layer.

  7. Sets the PxApplication on the Process Framework Task Tool extension.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.