Conductors (primary and secondary)

Object Model names: SPLITTARGET

ELECTRICNETWORKEDGE: You must assign this model name to any edge features in your electric network that will participate in the ArcFM Electric Next Upstream Protective Device and Isolation Protective Device traces.

FEEDERSECONDARY: Assign this model name if you want secondary conductors downstream of a transformer to inherit the transformer's LowSideVoltage or OperatingVoltage value.

Field Model names:

Field

Field Model Name

Properties

FeederID

FEEDERID

Field Info Tab:

Reset After Create = Yes

FeederID2

FEEDERID2

Field Info Tab:

Reset After Create = Yes

FeederInfo

FEEDERINFO

Field Info Tab:

Editable = No

Reset After Create = Yes

ElectricTraceWeight

MMELECTRICTRACEWEIGHT

Field Info Tab:

Reset After Create = Yes

OperatingVoltage

OPERATINGVOLTAGE

 

PhaseDesignation

PHASEDESIGNATION

 

Optional: The following field is required only if you have a multi-tiered network. The ParentCircuitSourceID or ParentCircuitSourceGUID field should exist on every feature class that participates in the multi-tiered network.

ParentCircuitSourceGUID

PARENTCIRCUITSOURCGUID

Field Info Tab:

Visible = Yes

Editable = No

Reset After Create = Yes

Add either ParentCircuitSourceGUID or ParentCircuitSourceID, but not both. If both are added, the feature will not work with the manager.

ParentCircuitSourceID

PARENTCIRCUITSOURCEID

Field Info Tab:

Visible = Yes

Editable = No<

Reset After Create = Yes

FacilityID

FACILITYID

Field Info Tab:

Visible = Yes

Editable = Yes

Reset After Create = No

Things to ensure for correct behavior:

  • FdrMgrNonTraceable is not set on features that you want to be traced

  • If you wish feeder manager to respect conductor phasing then a phase designation field is required for the edge, and the field must be driven by the phase designation domain (see previous step for instructions on setting up this domain)

  • Feeder Manager uses the voltage levels to determine continuity of phases when tracing though a transformer feature.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.