Submit Session

Changes the session’s status to Pending Approval and allows the user to assign it to an approval officer.

Enabled

  • MMSessionManager must be the current extension.

  • The selected node is a session.

  • The session must have been opened in ArcMap at least once.

  • If the session is open in ArcMap, the session must be editable and the user must have an editing session started.

Execute

  1. Prompts the user to save edits.

  2. Prompts the user to select an approval officer.

  3. Attempts to transfer ownership.

  4. Tells the builder that the user has changed so it can update the tree if necessary.

  5. If the session is open in ArcMap, it will be closed when it is submitted to another user.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.