Change Design’s Owner to Mobile User

Allows the user to change the owner of a design to a mobile user.

Enabled

  • MMWorkflowManager must be the current extension.

  • The node passed to this subtask must be a design.

  • Users must exist with the Mobile role assigned.

Execute

  1. Allows the user to select from a list of mobile users.

  2. Assigns design to the chosen user.

Parameters

  • DefaultUser: takes a user name as a value.

  • AutoChangeOwner: takes a value of 0 or 1. 0=False, prompt the user to select owner; 1=True, select default owner without prompt.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.